Skip to main content
hossam
Associate II
December 3, 2014
Question

g

  • December 3, 2014
  • 3 replies
  • 791 views
Posted on December 03, 2014 at 22:44

g

#hal_uart_error_pe-uart-parity
This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
December 4, 2014
Posted on December 04, 2014 at 17:50

Please don't do that, it damages the integrity of the forum

''Hi

 

 

I am using STM32F407 micro to implement UART communication with two HW modules using UART4 and UART5.

 

I used CUBE Mx to generate my code one of them is configures with 9 data bits and one parity bit ,send and receive in interrupt mode while the other is configured 8 data bits and no parity bits , send in polling mode and receive in interrupt mode

 

The Problem is That I a parity Error handler called from the 8data bits ISR?

 

IS that normal?, How can I avoid such problem?

 

 

Salam

 

Hossam Alzomor''
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
hossam
hossamAuthor
Associate II
December 4, 2014
Posted on December 04, 2014 at 19:20

Hi Clive,

I sent the post and the next day I discovered the cause of the problem, while my description of it was not accurate, I tried to remove the post but couldn't find a method on the forum to remove the post.

I removed the body body of the message and expected that will remove the whole message.

Amel NASRI
ST Technical Moderator
December 9, 2014
Posted on December 09, 2014 at 11:38

Hi Hossam,

I agree with Clive1.

The recommended practice is to edit or add a new post saying that the problem was resolved & if possible also tell other forum users what was the solution. This will be more helpful & very appreciated.

Welcome on our community!

-Mayla-

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.