STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Custom Bootloader STM32L151x

Posted on February 17, 2017 at 17:17Hi community,I would like to know if it's possible to create my own bootloader for STM32L151x.Where I could find info about it? Some code? Built-in code..?Thanks in advance.Regards#bootloader #stm32l151 #custom

Stm32F407VG USB Problem

Posted on February 18, 2017 at 09:17Hi,I am using STM32F407VG chip in my own PCB. I design MCU part of the PCB according to DISCOVERY board since it has the same controller. The board seems to work just fine. I tried ADC, DAC, SPI, USART, and simple...

0690X00000606KRQAY.png 0690X00000606C3QAI.png 0690X00000606KaQAI.png

I2C not working with usb

Posted on February 19, 2017 at 19:59Hello EveryoneI have a odd problem. I am using USB device to store data and reading data on same MCU(Slave) from other MCU(Master) on i2c but after after 2 or 3 transfer of data i2c stops working on slave mcu.What...

How to Debug FreeRTOS?

Posted on February 16, 2017 at 21:38I remodeled DemonstrationProgram of ST32Cube into STM32F746G-Discovery and was able to play the MP3 in audioplayer.My MP3Program may sometimes do Stall in Error.Will there be the good method to perform of Debug in...

STM32 DFU mode loads wrong driver (Total Phase)

Posted on February 14, 2017 at 02:48Hello,When I put my STM32F4 device into DFU mode, it is recognized as a ''Total Phase PD Analyzer Update Mode'' device instead of a ''STM Device in DFU Mode''. I can force using the STM DFU drivers, but by default...

0690X00000606GAQAY.png
JacobV by Associate II
  • 3540 Views
  • 6 replies
  • 0 kudos

F3 PWM inverted out: Cube bug?

Posted on February 16, 2017 at 17:45Using CubeMX I wanted to set four pins for PWM generation on an F302RCT, so it happened to get channels 1, 2, 3 and 4 on pins 27, 41, 44 and 45. Channels 2 and 3 fell on inverted output pins.When turning all pwm's...

AndreaC by Associate III
  • 730 Views
  • 0 replies
  • 0 kudos

USB pcd DMA not working

Posted on February 16, 2017 at 15:05Hi,I am using an STM32F7556NG microcontroller, connecting it to a host PC via USB, with the STM32 acting as a virtual COM port. Since the December 2016 release of the HAL, I have noticed a few strange things in th...

STM32F101 with StdPeriph_Lib

Posted on February 16, 2017 at 08:12Hi,I'm working on a new project, 2 boards: STM32F101CBT6 and STM32F101T6U6ATR.I've generated a project/code via Cube (which has many advantages), but, similar to other posts - the HAL layer is, simply, lot's of co...