STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

releaseMode is frozen (solved)

Posted on December 05, 2017 at 08:53Progrma is well work in debug mode but not in release mode.because of printf(' ');so I change'printf ('');' to//&sharpdefine DEBUG_MODE 0'&sharpifdef DEBUG_MODE printf(''); &sharpendif 'and then well work in relas...

To read multi-channel PDM signal

Posted on December 04, 2017 at 04:21Hi, I am working on a project that needs to read audio signal from 4 PDM microphones. I checked that STM32F405 chipset has 2 muxed full-duplex I2S. Is that mean I can read 4 channel audio data with this mcu? Is th...

Mao Zeng by Associate
  • 2133 Views
  • 3 replies
  • 0 kudos

Soft PWM?

Posted on December 04, 2017 at 23:33I need to update DAC in PWM.I have STM32F103C8T6 and two free timers (TIM3, TIM4).But they only have one global interrupt. How do I get PWM?I'm only called HAL_TIM_PWM_PulseFinishedCallback() and I get the meander...

0690X00000608xpQAA.png 0690X000006093rQAA.png 0690X00000608qtQAA.png

Is this the bug?

Posted on December 04, 2017 at 03:51 I use STM32 Cube to config USART2 to transmit data to computer. I don't enable USART2 Interrupt. I use DMA for USART2 Tx only (DMA1 Stream 6).uint8_t Data_to_send[5000]; __IO uint8_t Probe=0;int main(void) { HAL...

STM32f429 and USB_OTG_FS connections

Posted on December 01, 2017 at 09:40Hello STM members,Currently i am working on STM32f429 (144-LQFN) controller.For this project we have requiremnt USB_OTG_FS interface.I have query regarding USB OTG connections.1. Our system is working on 3.3v Now ...

STM32F1 FreeRtos Problem

Posted on December 03, 2017 at 07:32Hello.i using STM32F103 microcontroller,iar compiler and SPL libraryi tried to run FreeRtos on microcontrollerso i download FreeRtos Files From this link:https://sourceforge.net/projects/freertos/files/FreeRTOS/Fr...

[BUG] SDIO + RTOS (Stat = STA_NOINIT)

Posted on December 02, 2017 at 03:42 Hi, I just took two days to trace a bug that only appeared when I was doing concurrent reads & writes on my SD card from separate threads in FREERTOS. The bug is in sd_diskio.c and needs fixing intwo fun...

CubeMX - Static USBD setting?

Posted on November 29, 2017 at 18:27 Hi all, I've started a new F401 project, but for the life of me I cannot find the setting in CubeMX to have it create usbd_conf.h using the static malloc replacement: /* Memory management macros */ #def...

mwp by Senior
  • 1983 Views
  • 2 replies
  • 0 kudos

Resolved! how to set STM32 HAL FreeRTOS timer period?

Posted on August 09, 2017 at 15:21I am working with the HAL RTOS generated through cube and generally speaking, so far so good. I am used to using FreeRTOS but am a little stumped with this HAL RTOS, more specifically the timers. I have generated th...

I have a problem with FATFS

Posted on December 01, 2017 at 04:40I am working with STM32F407 Discovery Board and micro SD Card. I use STM32CubeMX version 4.23 to config SDIO 4 bit.This is my code to read data from micro sd card: FATFS myfatfs; FIL myfile; uint8_t SD_Data_Read_A...