STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 HAL_SPI_Transmit/Receive limitation

Posted on July 07, 2016 at 23:41version F4, 1.12 I am interfacing SPI to flash. calling HAL_SPI_Transmit or Receive alone disables SPI_DIRECTION_2LINES. I have to re-initialize it after each call. When using HAL_SPI_TransmitReceive. I have to specif...

alsaleem by Associate II
  • 863 Views
  • 2 replies
  • 0 kudos

Issues with STM32F4 USB bulk transfer (MIDI)

Posted on December 07, 2012 at 18:47Hi all,I'm working on an application for the STM32F4 where I need a USB MIDI device class. I've started with the STM USB library and, looking at the CDC and Audio class examples, have come up with a MIDI device th...

usb audio asynchronous prepare data out

Posted on June 30, 2016 at 11:25hi guys,I am doing usb audio asynch with stm32f072,my problem isUSBD_LL_PrepareReceive(pdev, AUDIO_OUT_EP, &PlaybackBuf[buftoogle],  AUDIO_MAX_PACKET_SIZE);My audio is 48Khz 24bit which will generate 288bytes so I set...

sgpiqx by Associate II
  • 830 Views
  • 1 replies
  • 0 kudos

Problem with UART interrupt STM32L031

Posted on July 01, 2016 at 12:50Hello xD,I have problem beacuse my stm32L031 is detect the 9200 baude and 1200 baude but after i do not get anything until I have to remain a card and soon several times to reset the card.In Part I initalisation initi...

ibrahim by Associate II
  • 541 Views
  • 0 replies
  • 0 kudos

STM32F4 Cube USB Device library

Posted on January 15, 2015 at 21:02Hi,I have created a HID class device using STM32F4 Cube USB device library.  Everything is working fine and I am able to exchange data with PC.  However, I would like to turn on/off an indicator LED when device is ...

Can I change UART baud rate in run time?

Posted on June 30, 2016 at 20:51Hello.STM32L1. I need change baud rate from 9600 to 115200 on run time.Which sequence?Now:1) Init port on 9600.2) Send command to GPS module for baud rate change to 115200.3) Reinit port on 115200.4) Overrun error rec...

dubanoze by Associate
  • 872 Views
  • 1 replies
  • 0 kudos

STM32 WiFi MAC Layer Modification

Posted on June 30, 2016 at 07:36Hi, I just start to use STM32F4 Discovery for real time network research using STM32F4 WiFi extension board. Some literature said that I have to modify the MAC Layer on network stack. My question is how to access the ...

rama by Associate
  • 527 Views
  • 0 replies
  • 0 kudos

HAL_I2C_MasterTxCpltCallback for second i2c

Posted on June 18, 2016 at 00:00I am using both I2Cs in my board. Also, using DMA for non-blocking.HAL_I2C_Master_Transmit_DMA generates interrupt for completion (also for reception and error.HAL only allows for one ''weak'' callback for both.Is the...

alsaleem by Associate II
  • 1240 Views
  • 1 replies
  • 0 kudos