STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FreeRTOS STM32F4 Question / Problem

Posted on December 23, 2017 at 21:40I am a beginner in both STM32 and FreeRTOS. I tried writing a FreeRTOS program logging ADC reading through serial port. I have a DMA set-up to save ADC readings in an circular buffer array, and I also have a DMA s...

0690X00000609HjQAI.png
Hz Lin by Associate II
  • 2310 Views
  • 4 replies
  • 0 kudos

USB CDC Bug in CubeMX firmware

Posted on April 11, 2014 at 10:07Hey everybody, in order to initialize a working Virtual Com Port with CubeMX on the STM32F4 Discovery, I had to change   pdev->pClassData = USBD_malloc(sizeof (USBD_CDC_HandleTypeDef)); to   pdev->pClassData = (void ...

STM32F302R6 and CAN

Posted on October 04, 2016 at 15:01 Hello. After the initialization CAN interface and call HAL_CAN_Receive_IT function (& hcan, CAN_FIFO0) there is no interruption USB_LP_CAN_RX0_IRQ Handler (); when receiving the CAN package. And accordingly mi...

ssurneed by Associate II
  • 2117 Views
  • 4 replies
  • 0 kudos

STM32CUBE vacant are not allowed to take the GPIO

Posted on December 26, 2017 at 15:11Hello Guys.I am working on the STM32FF417IGH6 Controller.I am having1)PSRAM2)Ethernet3)EMMC Device4) SPI1->LCD Display5)SPI2-> Other purpose6)Keypad 6x47) JTAG8) GPIOS for the LEDSNow when I am Allocating unused p...

deep ch by Associate II
  • 1289 Views
  • 1 replies
  • 0 kudos

STM32H7 DHCP Error

Posted on December 22, 2017 at 17:35I am using the STM32H743 NUCLEO-144, CubeMX V4.23.0, and CubeH7 V1.1.0.I do not see how DHCP can ever work using the CubeMX generated code. At the end of MX_LWIP_Init() is the only place where dhcp_start() is call...

MDS by Associate III
  • 902 Views
  • 0 replies
  • 0 kudos

Bug in USB HID, keyboard code

Posted on July 13, 2017 at 11:18I'd like to report a bug. In the file usbh_hid_keybd.c, ver. V3.2.2, date: 07-July-2015line 333:Now is: if(HID_Handle->length > (sizeof(keybd_report_data)/sizeof(uint32_t))){    HID_Handle->length = (sizeof(keybd_repo...

How to change USBH_malloc

Posted on November 06, 2017 at 15:59Hello,I`m using the CubeMX 4.23 and want to use the HAL USB Driver. In the usbh:conf.h is the code:/* Memory management macros */ &sharpdefine USBH_malloc malloc&sharpdefine USBH_free free&sharpdefine USBH_memset ...

tekampe by Associate II
  • 1741 Views
  • 3 replies
  • 0 kudos

Resolved! LwIP UDP updated examples ?

Posted on June 28, 2017 at 16:42Hello fellow stm32 explorersI am currently trying to communicate on a LAN network between a pc (server) and my stm32F4 discovery + phy module (client) via a UDP protocol.I am using LwIP with the RAW api (also called N...

andy b by Senior
  • 8310 Views
  • 3 replies
  • 0 kudos