cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L432KC HAL_PCDEx_BCD_VBUSDetect Bug

Rob.Riggs
Senior III
Posted on February 04, 2017 at 04:11

I am using CubeMX with the STM32L4 1.5.2 library. [EDIT -- just confirmed that this exists in 1.6.0 as well]

The non-OTG implementation of HAL_PCDEx_BCD_VBUSDetect() will only call  HAL_PCDEx_BCD_Callback() with PCD_BCD_DISCOVERY_COMPLETED if it detects a PCD_BCD_CHARGING_DOWNSTREAM_PORT.

The correct behavior should be to call HAL_PCDEx_BCD_Callback() with PCD_BCD_DISCOVERY_COMPLETED after any type of port is detected.

This is the relevant section of the defective code:

  /* If Charger detect ? */

  if (USBx->BCDR & USB_BCDR_PDET)

  {

    /* Start secondary detection to check connection to Charging Downstream

    Port or Dedicated Charging Port */

    USBx->BCDR &= ~(USB_BCDR_PDEN);

    USBx->BCDR |= (USB_BCDR_SDEN);

    HAL_Delay(300);

    

    /* If CDP ? */

    if (USBx->BCDR & USB_BCDR_SDET)

    {

      /* Dedicated Downstream Port DCP */

      HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_DEDICATED_CHARGING_PORT);

    }

    else

    {

      /* Charging Downstream Port CDP */

      HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_CHARGING_DOWNSTREAM_PORT);

      

      /* Battery Charging capability discovery finished

      Start Enumeration*/

      HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_DISCOVERY_COMPLETED);

    }

  }

  else /* NO */

  {

    /* Standard Downstream Port */

    HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_STD_DOWNSTREAM_PORT);

  }

This is what a correctly working version looks like:

  /* If Charger detect ? */

  if (USBx->BCDR & USB_BCDR_PDET)

  {

    /* Start secondary detection to check connection to Charging Downstream

    Port or Dedicated Charging Port */

    USBx->BCDR &= ~(USB_BCDR_PDEN);

    USBx->BCDR |= (USB_BCDR_SDEN);

    HAL_Delay(300);

    

    /* If CDP ? */

    if (USBx->BCDR & USB_BCDR_SDET)

    {

      /* Dedicated Downstream Port DCP */

      HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_DEDICATED_CHARGING_PORT);

    }

    else

    {

      /* Charging Downstream Port CDP */

      HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_CHARGING_DOWNSTREAM_PORT);

    }

  }

  else /* NO */

  {

    /* Standard Downstream Port */

    HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_STD_DOWNSTREAM_PORT);

  }

  /* Battery Charging capability discovery finished

  Start Enumeration*/

  HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_DISCOVERY_COMPLETED);

As an aside, it would be helpful if STM's HAL libraries were hosted in a public git repo so one could file a bug report and provide a pull request for the fix, rather than having to post this sort of thing in a public forum.  It is ill suited for reporting and fixing software defects.

#usb #bcd #stm32l4
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0