STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F107 Ethernet inicjalization

Posted on May 24, 2016 at 17:37 Hi, I am tring to initialize Ethernet with LWIP on STM32F To configure it I used CubeMX, but it can not pass this loop: /* Wait for software reset */ while (((heth->Instance)->DMABMR & ETH_DMABMR_SR) != (ui...

jakub2 by Associate
  • 1825 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F4 HAL Libaries

Posted on February 10, 2018 at 09:44Hi,I am trying to migrate from STM32 Standard peripheral libraries to HAL libraries. I have few queries here:1)   Can i use HAL libraries with Keil without first creating project in CubeMX? I just want to build my...

HAL_GPIO_EXTI_Callback with both USB and GPIO

Posted on February 05, 2018 at 13:23Hello, I'm facing a difficulty using CubeMx generated code with USB (CDC with VBus sensing).HAL_GPIO_EXTI_Callback is declared as 'weak' so for managing some GPIO's interrupts, I declared my own call back to 'catc...

Resolved! Bug in osMailCAlloc (cmsis_os.c)

Posted on May 29, 2017 at 16:50I believe there is a bug in the osMailCAlloc function from cmsis_os.c V1.02 (STM32Cube_FW_F1_V1.4.0).The function will always assign 0 to the first 4 bytes of the block, since sizeof an uint32_t is 4.if (p) {  for (i =...

kelvin2 by Associate
  • 1290 Views
  • 2 replies
  • 0 kudos

Resolved! LWIP - TCP connections are never closed

Posted on February 01, 2018 at 17:55Hello,I am developing a client-server system using an STM32F407 CPU.The client is a VB.net software that sends some commands to the server, opening and closing a TCP socket for every commands.To develop server fir...