STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SWD disabling after upload code to STM32F407VET6

Posted on February 25, 2018 at 00:21Hi.I wrote LED blinking code for STM32F407VET6.When I'm using Std_Periph_driver everything is fine. But when I write just CMSIS only led blinking code, after upload hex code to STM32F407VET6 code working, st-link ...

[F767ZI] Sampling and storing Measurement Data

Posted on February 16, 2018 at 01:03Hello!I want to start a project with the NUCLEO-F767ZI soon. In this project I want to measure some quantities with up to 100 kSamples/s and store the data.Would it be physically possible to have the data either s...

Armin L. by Associate II
  • 9770 Views
  • 29 replies
  • 0 kudos

STM32F769I-DISCO: No audio output from wm8994

Posted on October 14, 2017 at 03:33With STM32CubeF7 V1.8.0, there is no audio output from the wm8994 audio chip via the 3.5 mm blue audio output jack on the STM32F769I-Discovery board when parameter OUTPUT_DEVICE_HEADPHONE (or alias OUTPUT_DEVICE_HEA...

JB2500 by Associate III
  • 3607 Views
  • 4 replies
  • 0 kudos

USB OTG MSC B-L475 Board

Posted on February 24, 2018 at 11:09Hi,i have a B-L475 Board and i want to use USB OTG (Host) with a usb stick MSC.Under USB Host in CubeMX i have Drive_VBUS_Fs which Pin have i to choose?#usb-msc-device #stm32-l4

F407 and lis3dsh

Posted on February 23, 2018 at 15:01 I'm try use only registers for lis3dsh. https://community.st.com/external-link.jspa?url=https%3A%2F%2Fgithub.com%2Fmas-kon%2FF407-LIS3DSH - my code. This code sometimes is worked, but sometimes it stopped. C...

COM Port not detected on Windows 7

Posted on February 23, 2018 at 08:09Hello,I am using a STM32F072-EVAL with Atollic TruStudio IDE on Win7 x64 machine.I have started facing virtual com port cannot start (code 10) error since last 3-4 days. Have anyone faced this issue off late and m...