User Activity

Posted on February 13, 2018 at 18:23ST: Bug report:I've just upgraded from CubeMX V4.23.0 to V4.24.0.Using this re a Nucleo 144 'F767 board, I'm finding that 'Menu => Project => Generate Code' works once, then fails thereafter in one of two ways:If '...
Posted on October 14, 2017 at 03:33With STM32CubeF7 V1.8.0, there is no audio output from the wm8994 audio chip via the 3.5 mm blue audio output jack on the STM32F769I-Discovery board when parameter OUTPUT_DEVICE_HEADPHONE (or alias OUTPUT_DEVICE_HEA...
Posted on February 15, 2017 at 15:11  I've not been able to get the Audio Recorder in the demonstration software working. I'm using V1.2 of the software, as supplied with Cube V1.6.0.Test:Compile Demo V1.2 in Cube V1.6.0 using Eclipse 4.6.2 / Ac6 Sys...
Kudos from