STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is it possible to measure TTL signal levels at stm32L4 CAN pin Tx without being integrated into a can net?

Posted on March 08, 2017 at 14:25I'm using HAL_CAN_transmit to send data for stm32L4 mcu. I'm trying to send frames with 2 bytes in an infinite loop.I would like to know if it's possible and if feasible to measure TTL signal levels at GPIO TX pin of...

General Documentation for Ethernet PHY registers

Posted on March 07, 2017 at 17:54I am working on a board (STM32F407VGTx) that has an older PHY chip KSZ8721BL. I have similar code running on the MCBSTM32F400 (v1.2) which has an KSZ8081RNA. In testing, I retrieved all of the registers from both PHY...

dibs by Associate II
  • 1168 Views
  • 1 replies
  • 0 kudos

DMA with Storage_write_FS ?

Posted on March 05, 2017 at 07:29Hello everybody,How can I use DMA for this HAL_SD_WriteBlocks,I tried with HAL_SD_WriteBlocks_DMA, it doesn't work,Any clues ?Thanks======================int8_t STORAGE_Write_FS (uint8_t lun, uint8_t *buf, uint32_t...

quick usb question

Posted on March 05, 2017 at 12:01In simply words:I want to transfer data from PC via USB to STM32.I want to (somehow?) recognize data - some data should be saved to uint8_t Data1[20], and other data to uint8_t Data2[20].My question is:- should I cre...

John Doe1 by Associate III
  • 525 Views
  • 1 replies
  • 0 kudos

Resolved! jump from user application to custom bootloader

Posted on March 01, 2017 at 17:07Hi I have a custom bootloader that I flash to the first sector (0x8000000)  and when it receives a new program it loads it to 0x8003000. I can jumps to the user application,however  when It from user application jump...

USB MSC question ?

Posted on March 01, 2017 at 22:28♯Everybody,How can I configure USB MSC to work with my SDcard ?Which file is related ?Thanks#sdcard #configuration #stm32f103 #stm32cubemx #usb-msc

capture and play sound by STM32F407 and Codec

Posted on March 01, 2017 at 10:34Hi.I designed a PCB to use stm32f407 and TLV320AIC12 codec for capturing and playing sound.As you can see I connected I2S pin of stm to tlv in this way:STM32F407                   TLV320AIC12CK-----------------------...

nima2 by Associate II
  • 786 Views
  • 0 replies
  • 0 kudos