STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Release date of the STM32H7 LL (LowLayer) API?

Posted on March 20, 2018 at 10:38I found in a PDF document called ''STM32 Embedded Software'' following table where just ''2018'' is stated.Could ST give us please a more exact release date of the STM32H7 LL API (2018 Q2/Q3/Q4)?Thank you in advance....

0690X00000609uYQAQ.png
H S by Associate III
  • 1997 Views
  • 3 replies
  • 0 kudos

SPI Strange Output

Posted on June 09, 2018 at 00:05 Hello, I'm working on a project involving STM32L476RG Microcontroller. I'm trying to write a piece of code for creating an SPI Driver for my project and seem to have some issues. I'm using Keil v5 IDE. The output ...

0690X0000060LCtQAM.png

LwIP with SSH

Posted on June 12, 2018 at 10:52Hello,Knowing that I work with aSTM32 Cortex-M microcontroller by programming with Workbenche (Eclipse) under wndows, I would like to know if we could implement and add theSSH protocol to theLwIP stack ?Thank you all#...

Flash area Jtag couldn't download on?

Posted on June 12, 2018 at 04:15Hi. Recently I try to build bootloader. So I need to study about full programmable flash area.I'm using Jtag and IAR for debug, and STM32F103C8T6 for MCU, which has medium density flash area 0x0800 0000 ~ 0x0801 FFFF....

jd kim by Associate II
  • 1059 Views
  • 1 replies
  • 0 kudos

USB2642 Power Draw

Posted on June 11, 2018 at 15:01Hi,I am trying to build a daughter card using the USB2642 to provide two USB ports and a SD card slot to a processor board.   I am trying to do a minimalistic design that draws the least amount of power and smallest f...

USB compound device (hub) possible?

Posted on June 09, 2018 at 04:37I need to make a compound device, that's a multifunction device which looks like a hub with some devices behind it.  This is needed to work around a dumb host which does not understand composite devices.Is it possible...

Pavel A. by Super User
  • 934 Views
  • 0 replies
  • 0 kudos

Resolved! Firmware Update RAM requirements

Posted on June 08, 2018 at 16:22I'm looking to do some firmware updates over CAN bus on an M0 based part (possibly F091) which it looks like will require a custom bootloader. Do I need to pick a part with enough RAM to store the entire firmware imag...

Konami by Senior II
  • 2835 Views
  • 5 replies
  • 0 kudos