STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LwIP DHCP no ip request

Posted on July 11, 2017 at 18:17Hello fellow STM32 explorersI am currently working on a STM32F4 TCP/IP project.I'm using LwIP's RAW api.I got a echo UDP program working but with a static IP now I'm trying to get an ip adress automatically using a DH...

andy b by Senior
  • 1392 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L471 DFU

Posted on July 12, 2017 at 07:55I'm confused about wether STM32L471RG has a USB bootloader or not. AN2606 describes an STM32L47xxx DFU bootloader and that USB DM and USB DP lines should be connected to PA11 and PA12 respectively.But what confuses me...

0690X00000607H5QAI.png 0690X00000607YsQAI.png

playback wave file with DMA on STM32F745VGT6

Posted on July 11, 2017 at 17:23Hi Communities,I am using STM32F745VGTX Chip for my audio playing wave file application. My problem is that playing wave file takes too much processor power, therefore I want to use DMA instead. Is there any DMA mode,...

PC Connection detect using FTDI chip

Posted on July 06, 2017 at 15:40Hello,I am working on Stm32l073 series controller. I have small question regarding the deep sleep and exit from deepsleep modes when device is not plugged to PC i must make the device go to sleep. As the Block Diagram...

0690X00000607SkQAI.png
srm by Associate II
  • 1337 Views
  • 4 replies
  • 0 kudos

Code not going directly to main loop

Posted on June 22, 2017 at 11:16Hi,I am currently in the process of converting project code I have using the Standard peripheral library to the Hardware Abstraction Layer (HAL).I noticed that when I try to debug the code and place a breakpoint in th...

0690X00000607SQQAY.png 0690X00000607N2QAI.png

LwIP BYTE_ORDER compiler warning

Posted on May 23, 2017 at 02:09Hi,I am using CubeMX to generate a project using LWIP. The following files is added to my project which defines BYTE_ORDER:<project>/Middlewares/Third_Party/LwIP/system/arch/cpu.hThis define generates a compiler warnin...

STM32CUBE V4.21.0 LWIP Bug

Posted on July 04, 2017 at 08:14Hello everybody,i have found a bug in STM32Cube V4.21.0.I use the STM32F429BITxWhen i select the following settings the generated code have some RTOS functions. Please fix it.void MX_LWIP_Init(void){ /* IP addresses i...

0690X00000607JBQAY.png
mfrank9 by Associate III
  • 1007 Views
  • 3 replies
  • 0 kudos

STM32L0 - USB Configuration

Posted on July 04, 2017 at 17:44Hi,I am writing a firmware for a USB device that uses the STM32L052K8 microcontroller.Because my device must exhibit two USB interfaces, I have implemented a custom Composite Device class that acts like as broker: it ...