User Activity

Posted on March 16, 2018 at 11:32Hi,I have an STM32F1 Nucleo Development Board with a PowerStep01 Motor Drive IC.I have downloaded the X-CUBE-SPN3 source code from the following link on the ST website:<LINK NO LONGER ACTIVE>I copied the STM32F0 vers...
Posted on January 04, 2018 at 18:11Hi,I have just started working on a configuration wizard utility in Keil uVision for the setup of stepper motors.As can be seen, the configuration wizard so far setups the acceleration, deceleration, maximum and mi...
Posted on October 04, 2017 at 14:34Hi,I have recently just started working on Wi-Fi code on the SPWF01SA module using the STM32F1 Nucleo Development Board.I was able to get the various configuration values from the Wi-Fi module using the functions b...
Posted on June 22, 2017 at 11:16Hi,I am currently in the process of converting project code I have using the Standard peripheral library to the Hardware Abstraction Layer (HAL).I noticed that when I try to debug the code and place a breakpoint in th...
Posted on April 18, 2017 at 14:07Hi,When I am using the BEMF compensation configuration within the SPINFamily Evaluation Software, I input the Application Parameters and the Motor Parameters for my particular motor. When I press the �Evaluate� butto...