STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM Virtual Comm Port (VCP) driver slow on Windows 7

I have an STM32F4 device that uses the USB peripheral and CDC driver.I have a portable python app that communicates with the STM32F4 from Mac OS X 10.13 (High Sierra), Win10 and Win7.On Mac and Win10 the app communicates with good speed, however on W...

BSimo by Associate
  • 878 Views
  • 0 replies
  • 0 kudos

Bug on SDcard and stm32f415 ?

Hi, i have a problem with my project....I'm using Fat and SD with freertos to read/write files on SD using hdma channel.First part i fixed all "SDIO_STA_STBITER" with "SDIO_STA_STBITERR" (with 2 "R" ) because a typo is present.But i see the interrupt...

Marco1 by Associate II
  • 4448 Views
  • 9 replies
  • 0 kudos

['F407 OTG] Is OTGx_HPRT.PENA rc_w0?

In RM0090 rev.17 both OTG_FS and OTG_HS, the HPRT.PENA is described as rc_w0.However, the code in Cube does not support this; rather, it seems it's rc_w1.RM0390 says it's rc_w1, and although it's a slightly different revision of the OTG core, I'd say...

STM32F072B-Discovery TSC Cube Project

I try to generate TSC project by using STM Cube,but I am not sure how to write this function: void HAL_TSC_ConvCpltCallback(TSC_HandleTypeDef* htsc).There is same function in "STM32Cube\Repository\STM32Cube_FW_F0_V1.9.0\Projects\STM32F072B-Discovery\...

STM32L152 Bootloader Extended Erase Failure

Using our internally developed tool for writing a binary to a target using the in-ROM Bootloader according to AN3155 and AN2606, we were unable to appropriately perform commands as described in both application notes, specifically Bootloader Extended...

CVoro by Associate II
  • 1652 Views
  • 2 replies
  • 0 kudos

Resolved! HTML documentation for LL and HAL

I remember a couple of years ago, at least, that ST had documentation for HAL and LL drivers in the form of html pages like they do for the CMSIS documentation. They were great for quickly getting the info that I needed.Does anyone know if they are s...

Resolved! Stm32 HAL library timer

Hi guys,So I used an example of the HAL library to configure an input capture with a timer on a stm32f373vct6 microcontroller.Now I want to include this example in my project, but when I do so and try to build the compiler says :Error: L6218E: Undefi...