STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 USB HOST HID problem

Posted on August 04, 2017 at 16:47I'm rather new in USB domain and I'm using ST std periph library and STM32_USB-Host-Device_Lib_V2.1.0 (and V2.2.0) on STM32F4 (my own board and STM32F407 Discovery). I've tested MSC host and it works fine but about ...

0690X00000607kqQAA.png

CMSIS - pros and cons

Posted on August 04, 2017 at 10:40Hi,We're entering a new project with STM32F7676 and thinking about which RTOS to use. Our [initial] understanding is that CMSIS is a set of standardized APIs to peripherals, driver and to an actual RTOS implementati...

RTOS config from CubeMX not working

Posted on June 26, 2017 at 10:17Hi, I am new to putting together my own projects and have followed this http://www.carminenoviello.com/2015/06/22/running-freertos-stm32nucleo-free-gcceclipse-toolchain/&sharpcomment-78392 great write up, adapting the...

USB FS CDC

Posted on August 03, 2017 at 13:53I try to make a USB CDC HOST FS with an Nucleo STM32F746ZG but,I made the project with CubeMx and when i plug my device the enumeration work, i can see it with a beagle usb but i don't reach the HOST_USER_CLASS_ACTI...

Resolved! Getting an interrupt at specific encoder value

Posted on July 31, 2017 at 14:41Beginner working with STM32L452:I have TIM2 set up as encoder-based timer. Works perfect.Now I want an interrupt whenever the TIM2 reaches a certain value (position).I tried to enable timer interrupt through HAL_TIM_E...

Krix N by Associate II
  • 1739 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F756 USB and WFI

Posted on July 27, 2017 at 09:55I have a problem with STM32F756 USB CDC (HS with FS PHY) device and core sleeping. I isolated all other code and left only the USB driver and main loop calling WFI instruction. If there is no call to WFI, USB is worki...