cancel
Showing results for 
Search instead for 
Did you mean: 

CMSIS - pros and cons

Roy Ben Hayun
Associate II
Posted on August 04, 2017 at 10:40

Hi,

We're entering a new project with STM32F7676 and thinking about which RTOS to use.

Our [initial] understanding is that CMSIS is a set of standardized APIs to peripherals, driver and to an actual RTOS implementation. Seems that the CMSIS solution is being strongly promoted (over using an RTOS w\o CMSIS).

As for the RTOS - seems we can pick from either CMSIS+RTX or CMSIS+FreeRTOS (?) or FreeRTOS w\o CMSIS.

Few basic questions on CMSIS itself:

- does CMSIS simply map APIs to the RTOS or does it actually add a layer of intermediate code?

- what overhead (e.g., code and size) does CMSIS add on top of the underlying RTOS?

- what additional dependencies are added when using CMSIS?

A couple of question on CMSIS + an RTOS:

- any pros and cons using CMSIS-RTX vs CMSIS+FreeRTOS?

- what are the pros and cons using CMSIS+FreeRTOS vs FreeRTOS w\o CMSIS?

Thanks!

--roy

#cmsis-rtos #stm32-freertos
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0