STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32N6 DK ETH problem

I use STM32Cube FW_N6 V1.2.0 to create an FW to run a web server on the DK board. I figured out that I can not talk to the PHY chip to read the PHY ID. I compared the code with another example that ST released and figured out that these codes are mis...

AliR by Associate
  • 569 Views
  • 2 replies
  • 1 kudos

DMA2D minimum width requirement?

Hello,I'm using a H743 with the DMA2D device in RegToMem mode.  Generally it seems to work for larger images, but I've been trying to fill a small rectangle (5 x 60) pixels, and I was expecting 300 write pulses.  Instead, I'm getting 480 pulses (8 x ...

matt-crc by Senior III
  • 471 Views
  • 2 replies
  • 0 kudos

CAN RX ring buffer interrupt

I am simulating messages to be received via CAN on the STM32F0xx series uC. The hardware FIFO does not overflow as I have activated the overflow interrupt and checked the FIFO level, which never exceeds 1. The current implementation consists of a 128...

Resolved! My STM32 Code only works under debug mode

#include <stdint.h> #include <stdio.h> #include "stm32f4xx.h" volatile uint8_t rxdata = 0; int main(void) { SystemInit(); SystemCoreClockUpdate(); // clock configutation RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); // TX: PB6 RX: PB7 RCC...

XY by Associate II
  • 1327 Views
  • 10 replies
  • 7 kudos

STM32F407 USB Host config for FT232RL

Title edited to name the device being hosted. Hello , I am currently trying to configure STM32F407 board as USB host. The code for it is given below. I am not receiving anything from the USB device(bus powered). I have a doubt that it might be relat...

SohamC by Associate III
  • 2866 Views
  • 22 replies
  • 8 kudos

Resolved! Ethernet Ping not working in NUCLEOH753ZI

I am using Nucleo STM32H753ZI board. The STMCube IDE version is 1.19.0 and FreeRTOS version is 1.3.1 and CMSIS RTOS1 version is 1.02 I have enabled Icache, DCache and MPU. Integrated the stacks of LWIP,Ethernet and FreeRTOS too.Basic ping functionali...