STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

free ModBus on STM32F767

Hello friends.I try imeplement freemodbus on my project. And I have a problem with connect. My task is here:/* ------------------------ Defines --------------------------------------- */   #define REG_INPUT_START 1000 #define REG_INPUT_NREGS ...

Resolved! DFU Serial Number

I am looking at the code here that has the algorithm for producing the device serial number reported when the MCU is in USB DFU mode.https://github.com/libopencm3/libopencm3/blob/master/lib/stm32/desig.cThe document they reference there, https://my.s...

How forward data from COM PORT to UART

I want to forward all data received at the VCP with USB FS to UART how can i implement this specific in code?I have been searching for long time for this and i have not found any good example of it.Can you please help me?Until now i am doing this lik...

arduo by Senior
  • 1776 Views
  • 1 replies
  • 0 kudos

Resolved! Forward Data from VCP to UART

How can i forward data which i received at my COM Port via USB FS to a UART of my Choice?I already send data to UART5 and i measured it with an osci and its workinghar buffer[] = "TEST"; HAL_UART_Transmit(&huart5, buffer, sizeof(buffer), HAL_MAX_DELA...

arduo by Senior
  • 1669 Views
  • 7 replies
  • 0 kudos

Using USB device Virtual comm questions

Hello, Using CubeMX, I have created USB CDC device for FS and started using the CDC.By modifying CDC_Receive_FS() I am able to receive all data sent form the PC over USB and put the data in my bufferAlso (while the USB cable is connected and PC term...

STM32F769 Discovery Board

I am currently trying to use the DFU mode on the STM32F769 Discovery Board. I have shorted a connection to VCC to pull BOOT0 to 3.3V (From Schematic R19). I have wired up PA11, PA12 and ground (Using USB pins) to the arduino connector on the board...

IAgui by Associate III
  • 1236 Views
  • 2 replies
  • 0 kudos

Can't get the STM32H7 USB audio HS example to work

Hi there, I've got a new STM32H743I EVAL board and am trying to run the USB audio HS example provided with stm32cube_fw_h7_v130.The Full-speed example works fine.I'm using the correct USB connector, my PC (Windows 10) recognises the device and says i...

Mttjcksn by Associate III
  • 1432 Views
  • 2 replies
  • 0 kudos