STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STSAFE AWS IoT Demo

I have found ST presentation regarding "STSAFE AWS IoTDemo" https://www.st.com/content/ccc/resource/sales_and_marketing/presentation/application_presentation/group0/28/06/3d/89/9d/86/4d/0d/IoT_World_2017_Cloud_Demo/files/IoT_World_2017_Cloud_Demo.pd...

ritesh by Associate II
  • 915 Views
  • 0 replies
  • 0 kudos

STM32F765ZI USB problem.

Hello, I am using stm32f765ZI controller in my project, where i have the application to communicate to PC using USB.I have generated USB code from cube MX with USB clock speed 48 MHz and enabled full speed device only.But in device manager it is show...

Correct method of using CDC (Virtual Com Port)

Hi there,I love using Cube and being able to get a project up and running super quickly, especially because I work in an agile development environment.I am using CDC/USB/VCP for the first time on an STM32 system (STM32F070RB specifically, FYI) and wa...

0690X000006DoKzQAK.jpg
SWill.10 by Associate II
  • 873 Views
  • 0 replies
  • 0 kudos

STM32_USB_OTG_Driver v2.2.0 Availability

Hello, I am working on STM32F412 controller. We are using a previous version of the OTG driver v2.2.0 on which our most of the development works are done. We are on course of reviewing the changes on our application layer that we have developed, but ...

Possible SPI DMA bug in STM32K743IIK

I've run across what looks like a bug in the STM32H743IIK (144pin BGA) related to SPI DMA. It is a very strange one, and you can see the history of this issue on the ChibiOS forums here:http://www.chibios.com/forum/viewtopic.php?f=16&t=4140&start=80I...

tridge by Associate II
  • 2879 Views
  • 6 replies
  • 0 kudos

Resolved! I can only write to SD card once (SPI-fatfs)

I am using a stm32f407 and i use this code inside a loop:/* Mount SD Card */ if(f_mount(&fs, "", 0) != FR_OK) _Error_Handler(__FILE__, __LINE__); /* Open file to write */ if(f_open(&fil, "first.txt", FA_OPEN_ALWAYS | FA_READ | FA_WRITE) ...

NBlac by Associate III
  • 1957 Views
  • 2 replies
  • 0 kudos

External Flash of STM32L4 Through Boot Option

Hello:I wish to understand how to set up the hardware on an STM32L476Rxx device so I can flash the controller through a serial port. Is there documentation to support this, such as an app note? (unable to find anything) Any help is appreciated. Than...