2019-02-23 9:32 AM
I am using a stm32f407 and i use this code inside a loop:
/* Mount SD Card */
if(f_mount(&fs, "", 0) != FR_OK)
_Error_Handler(__FILE__, __LINE__);
/* Open file to write */
if(f_open(&fil, "first.txt", FA_OPEN_ALWAYS | FA_READ | FA_WRITE) != FR_OK)
_Error_Handler(__FILE__, __LINE__);
/* Check free space */
if(f_getfree("", &fre_clust, &pfs) != FR_OK)
_Error_Handler(__FILE__, __LINE__);
total = (uint32_t)((pfs->n_fatent - 2) * pfs->csize * 0.5);
fre = (uint32_t)(fre_clust * pfs->csize * 0.5);
/* Free space is less than 1kb */
if(fre < 1)
_Error_Handler(__FILE__, __LINE__);
/* Writing text */
sprintf(counter_buff, "%.10f", count);
f_puts("\n", &fil);
f_puts("STM32 SD Card I/O Example via SPI\n", &fil);
f_puts(counter_buff, &fil);
f_puts("\n", &fil);
/* Close file */
if(f_close(&fil) != FR_OK)
_Error_Handler(__FILE__, __LINE__);
/* Open file to read */
if(f_open(&fil, "first.txt", FA_READ) != FR_OK)
_Error_Handler(__FILE__, __LINE__);
while(f_gets(buffer, sizeof(buffer), &fil))
{
//printf("%s", buffer);
}
/* Close file */
if(f_close(&fil) != FR_OK)
_Error_Handler(__FILE__, __LINE__);
/* Unmount SDCARD */
if(f_mount(NULL, "", 1) != FR_OK)
_Error_Handler(__FILE__, __LINE__);
HAL_GPIO_TogglePin(GPIOE, GPIO_PIN_0);When i open the file from the sd card on my pc i only see this:
1.35
STM32 SD Card I/O Example via SPI
1.35
The led keeps on toggling so the code is running.
Any ideas?
thanks
Solved! Go to Solution.
2019-02-23 10:45 AM
What is it supposed to do in your mind?
If you want it to add lines, perhaps f_seek() to the end of the file.
How does the count advance? Is it really a float?
if (f_open(&fil, "LOG.TXT", FA_OPEN_ALWAYS | FA_WRITE) == FR_OK)
{
UINT BytesWritten;
const char string[] = "Another line gets added\r\n";
f_lseek(&fil, f_size(&fil));
f_write(&fil, string, strlen(string), &BytesWritten);
f_close(&fil);
}
2019-02-23 10:45 AM
What is it supposed to do in your mind?
If you want it to add lines, perhaps f_seek() to the end of the file.
How does the count advance? Is it really a float?
if (f_open(&fil, "LOG.TXT", FA_OPEN_ALWAYS | FA_WRITE) == FR_OK)
{
UINT BytesWritten;
const char string[] = "Another line gets added\r\n";
f_lseek(&fil, f_size(&fil));
f_write(&fil, string, strlen(string), &BytesWritten);
f_close(&fil);
}
2019-02-23 11:24 AM
I thought that just by adding "f_puts("\n", &fil);" it would change line and next data would be written after that. But now i realized it doesn't. I used your code for writing to the card and it works great.
thanks a lot