STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bug in STM32L4xx_HAL_Driver, QUADSPI

Posted on May 04, 2018 at 11:24Hi,I found a bug in the quad spi driver for stm32l4xx. In the function  HAL_QSPI_Receive_IT, the interrupts flags must be cleared before start transfer otherwise flag TC could be missed:- WRITE_REG(hqspi->Instance->AR,...

Can't build STM32F746 Discovery + LwIP project

Hi everybody,I created a project for using the STM32F746 DISCOVERY board with LwIP utility (see image 1 and Image 2).  As soon as the project gets created i tried to build it, but ended up not beeing able to do so and getting the error shown in image...

MEsco by Associate II
  • 1363 Views
  • 0 replies
  • 0 kudos

Can't Open COM Port

I am using USB Virtual Com Port with CubeMX on a STM32F4 controller.The problem is, that occasionally, but increasingly often I cannot open the COM Port to my Device. It is very hard to reproduce, as changes in completely different code regions can c...

arduo by Senior
  • 2158 Views
  • 2 replies
  • 0 kudos

Does HAL_FLASH_OB_Launch() result in a reset?

Hi ,I am using STM32L series of MCU.From the application code independent watchdog is used and when it is time for entering bootloader say due to firmware upgrade, i use while(1) to reset the system.1.Once inside bootloader I am observing that the bo...

How to use USB HS?

Hi there,i have Projects where I used USB FS for COM Port Communication. How can i change them to USB HS do i need to change the clock or other settings?Thanks in advance.I am new with STM32

arduo by Senior
  • 1189 Views
  • 1 replies
  • 0 kudos

STM32F303 ADC doesn't run, advice welcome!

Hi all,The ADC on my STM32F303 doesn't want to run. I'm trying to measure 8 input channels via DMA with TIM7 as the ADC trigger. Having had a thorough read of the examples in the repo for Cube, my setup should work but it doesn't. The values never ch...

STSAFE AWS IoT Demo

I have found ST presentation regarding "STSAFE AWS IoTDemo" https://www.st.com/content/ccc/resource/sales_and_marketing/presentation/application_presentation/group0/28/06/3d/89/9d/86/4d/0d/IoT_World_2017_Cloud_Demo/files/IoT_World_2017_Cloud_Demo.pd...

ritesh by Associate II
  • 893 Views
  • 0 replies
  • 0 kudos

STM32F765ZI USB problem.

Hello, I am using stm32f765ZI controller in my project, where i have the application to communicate to PC using USB.I have generated USB code from cube MX with USB clock speed 48 MHz and enabled full speed device only.But in device manager it is show...

Correct method of using CDC (Virtual Com Port)

Hi there,I love using Cube and being able to get a project up and running super quickly, especially because I work in an agile development environment.I am using CDC/USB/VCP for the first time on an STM32 system (STM32F070RB specifically, FYI) and wa...

0690X000006DoKzQAK.jpg
SWill.10 by Associate II
  • 854 Views
  • 0 replies
  • 0 kudos