STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB CDC Class problem

Posted on February 26, 2018 at 10:02Hi,I am working on a nucleo STM32H7 and I am trying to communicate with a Hokuyo through USB. When  I connect the device  the init fails at some point in the usbh_cdc.c (USBH_CDC_InterfaceInit)In this function the...

ab val by Associate III
  • 833 Views
  • 1 replies
  • 0 kudos

Knowing when USB CDC is ready to tx

Posted on May 05, 2018 at 02:46Context.  I using CubeMx on a STM32L462 with FreeRTOS (works fine).  When enabled, MX_USB_DEVICE_Init() is added to the default FreeRTOS task to activate a USB channel which also works fine.. I have my USB channel set ...

STM32F429 Disco1 HOST HID

Posted on December 14, 2017 at 08:16Code Generator using cubeMX for STM32F429 Disco1 HOST HID.Keyboard Behavior:When I connect Keyboard, It Shows that keyboard is connected. But If I press any key on keyboard. Immediately USB disconnected routines s...

STM32F103 ADC + DMA multichannel, from FreeRTOS software timer. Continuous mode works. Manually triggering HAL_ADC_Start_DMA() return HAL_ERROR on ADC_Enable() on second call

Posted on February 21, 2018 at 19:20Hi,I've successfully run a FreeRTOS program that use ADC + DMA in scan, continuous, circular mode and I successfully can average in HAL_ADC_ConvCpltCallback().Now I'd still like to use DMA to fill a buffer of 3 ch...

HAL I2C slave busy

Posted on April 18, 2018 at 11:23I'm trying to use the I2C slave in DMA mode.uint8_t aRxBuffer;HAL_I2C_Slave_Receive_DMA(&hi2c1, (uint8_t*)&aRxBuffer, 1);But HAL_I2C_Slave_Receive_DMA returns HAL_BUSY.At the same time I have no other devices on the ...

Looking for PPP example for lwIP

Posted on September 12, 2017 at 23:36Hi,I'm currently trying to find an example project for that run PPP on LwIP with STM32F407 based card with sim800H GSM modem.Best Regards.#ppp #gsm-modem #lwip