cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407ZGT Ethernet DP83848 RMII ''unidentified network''

Posted on April 11, 2018 at 07:17

Hi , Im working on STM32F407ZGT in my custom made PCB, Im working on Ethernet with DP83848i PHY in RMII mode, I downloaded the STMcube ethernet template code for  

DP83848 MII mode, I changed the code according to RMII requirements. But still it is not working, Im seeing my device as 'unidentified network' trying to sort, I have to be sure that my code is a working code. STM mcu is successfully communicating to

DP83848

 registers. Since Im turning LED on when Ethernet is connected. 

Regarding Hardware connection, 

50Mhz Osc -> DP X1

Stm TxEn -> DP TxEn

Stm TxD0 -> DP TxD0

Stm TxD1 -> DP TxD1

Stm RxD0 -> DP RxD0

Stm RxD1 -> DP RxD1

Stm CRS_DV -> DP CRS_CRSDV

Stm MDIO -> DP MDIO

Stm MDIO_CLK -> DP MDC

Stm RMII_REFCLK<-DP X1

In Code I tried with Static IP

                        MY computer                   STM32F407

ip->                  192.168.0.5                      192.168.0.

5

Mask->             255.255.255.0                  255.255.255.0

gateway->         192.168.0.1                     192.168.0.1

After updating the Firmware and connecting Ethernet crossover cable , 

LED_SPEED -> Always LOW (LED ON)

LED_LINK -> Always 

LOW (LED ON)

LED_ACT->Changing from 3.3 V to 1.8 V

Can I get  a example code for LWIP_HTTP_Server_Raw for DP83848 RMII mode.

Thanks in advance

#rmii #etherent #lwip #dp83848 #raw-lwip #http-server #stm32f4 #stm32f407
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Sorry, bumping old zombie unanswered threads off my feed

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..