STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB CDC Change Device name

Posted on April 28, 2017 at 12:29Hey,i use the STM32F4 USB CDC (generate by CUBEMX(v.4.20)) and want change the shown name in the Device Manager.I change these lines but nothing change in the device manager.&sharpdefine USBD_VID     1155&sharpdefine...

HAL_SPI_Transmit on F0, F1, F4, F7

Hi!I have module for transmit dates to SPI Interface.Data is - pointer to data buffer uint8_t.In F1 & F4 all will be ok.But in F0 & F7 modules will send *((uint16_t *)pData) (see modules below)Program for F1 or F4 will not work on F0 & F7.Where error...

VLev by Associate II
  • 6081 Views
  • 17 replies
  • 0 kudos

No LL CAN code in F7 Cube ?

I downloaded the latest F7 Cube package, V1.15.00, to get the LL CAN driver code for the F74x But there is none.And the F74x is not that new, I think this is not supposed to change. Is it so ?Guess I need to switch to the SAME70 XPLD board.

AvaTar by Lead
  • 933 Views
  • 0 replies
  • 0 kudos

BUGs in STM32F0xx_StdPeriph_Lib_V1.5.0

I have been implementing firmware for STM32F042 and used the Std Peripheral library (v.1.5.0). I found the following bug(s):Bug: DMA1_Channel4_5_IRQn() was never calledIn file Libraries/CMSIS/Device/ST/STM32F0xx/Include/stm32f0xx.hLine 5558:#define D...

MArgi by Associate II
  • 2313 Views
  • 3 replies
  • 0 kudos

CubeMX - Full duplex communication in USB CDC

Posted on April 24, 2015 at 16:30 So, I have finally achieved sending capability over CDC USB. BUT... I have this CDC_Receive_FS function /** * @brief CDC_Receive_FS * Data received over USB OUT endpoint are sent over CDC interface *...

sincoon by Associate III
  • 4540 Views
  • 8 replies
  • 0 kudos

Bootloader for STM32f469-DISCO

Hello!I am trying to program a bootloader so that it loads directly my application (.bin) through the USB in the electronic card STM32F469-DISCO but it does not work for me. I would like to know if there is a generic bootloader that I can download to...

FFran by Associate II
  • 1430 Views
  • 2 replies
  • 0 kudos

STM32F767ZI + USB host + FatFS problem

Hello,I'm using the STM32F767ZI and I'm using the FatFS feature with USB host communication. I created a project based on the example provided by STM32 CubeMX.The program works. I can read in one file and write in another. My problem happens when I w...