STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C3 Bus Busy issue!

Dear friends,I am trying to read data from DS3231 RTC using SPI3 peripheral of STM32407VGt6 MCU.At first I used the latest version of HAL drivers and Cube and easily could read/wrtie the DS3231 RTC module. But now I need to use Standard Peripheral li...

Mujtaba by Senior
  • 5499 Views
  • 13 replies
  • 0 kudos

STM32L010K8 Flash WRPERR error

I am using an STM32L010k8 device, every second word write to Flash using the HAL driver function HAL_FLASH_Program() generates a write protection fault (WRPERR bit in FLASH_SR). If I retry the write to the same address the error is not presentIs this...

SThom.7 by Associate III
  • 1864 Views
  • 2 replies
  • 0 kudos

STM32F7 HAL Slave RX behavior is strange.

I found very strange behavior of the STM32F7 HAL I2C. Please see the description below. I have also attached problem demonstration program and screenshot.Regards,Seiichi CubeMX version 5.0.0 for LinuxSW4STM32 version 1.15.0.201708311556 for Linux 64b...

Takemasa by Associate III
  • 2095 Views
  • 1 replies
  • 0 kudos

Resolved! What is the relationship between the DAC dataholding registers, data output registers, and the conversion half/full complete callbacks?

Hello everyoneI am having trouble understanding the relationship between the registers and the callback functions for my application. Briefly put, I am transferring 2 values to the DAC via DMA using TIM6 as interrupt at a rate of 50 Hz. I want to sam...

0690X00000881HkQAI.png 0690X00000881HzQAI.png 0690X00000881I9QAI.png 0690X00000881ITQAY.png

Resolved! STM32L4R9I-EVAL demo source code

​Could you provide demo source code on the board STM32L4R9I-EVAL. I bought the STM32LR9I-EVAL board and the current demo program is very cool. I need the demo source  code to study. Thanks!

ZXu.6 by Associate
  • 1667 Views
  • 2 replies
  • 0 kudos

Resolved! HardFault_Handler from stm32 + Fatfs + USB

Hello,A project created in truestudio generates a HardFault_Handler.There are 2 PCBs I made. PCB A and PCB B are the same circuit and components. I have confirmed that the operation is correct while writing the code in PCB A.However, there was a prob...

SWoon by Associate II
  • 2195 Views
  • 3 replies
  • 0 kudos