STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CubeMX - Full duplex communication in USB CDC

Posted on April 24, 2015 at 16:30 So, I have finally achieved sending capability over CDC USB. BUT... I have this CDC_Receive_FS function /** * @brief CDC_Receive_FS * Data received over USB OUT endpoint are sent over CDC interface *...

sincoon by Associate III
  • 4373 Views
  • 8 replies
  • 0 kudos

Bootloader for STM32f469-DISCO

Hello!I am trying to program a bootloader so that it loads directly my application (.bin) through the USB in the electronic card STM32F469-DISCO but it does not work for me. I would like to know if there is a generic bootloader that I can download to...

FFran by Associate II
  • 1371 Views
  • 2 replies
  • 0 kudos

STM32F767ZI + USB host + FatFS problem

Hello,I'm using the STM32F767ZI and I'm using the FatFS feature with USB host communication. I created a project based on the example provided by STM32 CubeMX.The program works. I can read in one file and write in another. My problem happens when I w...

I2C3 Bus Busy issue!

Dear friends,I am trying to read data from DS3231 RTC using SPI3 peripheral of STM32407VGt6 MCU.At first I used the latest version of HAL drivers and Cube and easily could read/wrtie the DS3231 RTC module. But now I need to use Standard Peripheral li...

Mujtaba by Senior
  • 5296 Views
  • 13 replies
  • 0 kudos

STM32L010K8 Flash WRPERR error

I am using an STM32L010k8 device, every second word write to Flash using the HAL driver function HAL_FLASH_Program() generates a write protection fault (WRPERR bit in FLASH_SR). If I retry the write to the same address the error is not presentIs this...

SThom.7 by Associate III
  • 1812 Views
  • 2 replies
  • 0 kudos

STM32F7 HAL Slave RX behavior is strange.

I found very strange behavior of the STM32F7 HAL I2C. Please see the description below. I have also attached problem demonstration program and screenshot.Regards,Seiichi CubeMX version 5.0.0 for LinuxSW4STM32 version 1.15.0.201708311556 for Linux 64b...

Takemasa by Associate III
  • 2022 Views
  • 1 replies
  • 0 kudos

Resolved! What is the relationship between the DAC dataholding registers, data output registers, and the conversion half/full complete callbacks?

Hello everyoneI am having trouble understanding the relationship between the registers and the callback functions for my application. Briefly put, I am transferring 2 values to the DAC via DMA using TIM6 as interrupt at a rate of 50 Hz. I want to sam...

0690X00000881HkQAI.png 0690X00000881HzQAI.png 0690X00000881I9QAI.png 0690X00000881ITQAY.png