STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to disable a STM32 UART interrupt?

I know one can enable a UART receive interrupt using HAL_UART_Receive_IT(&huart2, (uint8_t *)rx_buffer, expectedNumberOfBytes)But once started how does one stop it, "manually"?We can disable the UART interrupt using HAL_NVIC_EnableIRQ . This will ...

CJohn.7 by Associate II
  • 6745 Views
  • 5 replies
  • 0 kudos

Change Timer and PWM period "on the fly" ?

Hi, I'm currently trying to set up acceleration and deceleration phases for a stepper motor. For that I'm tryin to change the frequency of the PWM [timer1] ( and the Timer [TIMER1] interrup associated). I'm working on a STM32F407-DISC. I found out t...

JTurp by Associate II
  • 2585 Views
  • 2 replies
  • 0 kudos

How can I use a Raspberry Pi to update the firmware on an STM MCU? Also, which families of STM are capable of going through such a process?

I want to update the firmware on an STM using a raspberry pi 3 that has been connected to it. How can I do so? Please help me with the names of the families of STM that are capable of going through with this process. Also, can this be done using the ...

SSoni by Associate III
  • 2977 Views
  • 3 replies
  • 0 kudos

Assertion "pbuf_free: p->ref > 0" failed at line 747 ../Middlewares/Third_Party/LwIP/src/core/pbuf.c Received too many bytes! Droping client.

Hello Everyone,I am using STM32F429ZIT MCU and Modbus TCP library provided by FreeModbus.After attaching TCP library to my application code, i am getting below errors.In modbus TCP library , inside portTCP.c , if i am commenting prvvMBPortReleaseClie...

0690X00000896dsQAA.png 0690X00000896egQAA.png