STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 USB CDC not working for F0, F4 boards

I have tried USB examples for Stm32F070, F401, F407 Black board and calling a single "CDC_Transmit_FS" function to print a string but none is working. The hcdc->TxState value is some garbage big value so it always stay busy and also not getting inter...

Lakshay by Associate
  • 612 Views
  • 1 replies
  • 0 kudos

Resolved! CMSIS-DSP rfft init throwing an error

STM32WB55arm_rfft_fast_instance_f32 fft_instance; arm_rfft_fast_init_f32(&fft_instance, NUM_SAMP);I'm trying to use the rfft_fast function from the arm_math.h libraryBut when I compile I get... ../STM32_WPAN/App/custom_app.c:122:24: error: expected d...

Resolved! STM32F446 - SPI DMA

What's wrong with my code? Every time I start a DMA transfer only 2 Bytes get transferred although I specified 16 bytes.Also, I get an FIFO Error after transmit, whereas Transmit Complete is ok./* FUNCTION ************************************/ void S...

Resolved! Misunderstanding the STM32F7 boot process

Hi,I attempt to free the 1st sectors of the MCU flash by relocating the firmware and its interrupt vector table to further sector (e.g sector 5 at 0x08040000 address). For that purpose, I updatedthe linker (IAR) configurationthe vector table location...

TPier by Associate III
  • 671 Views
  • 3 replies
  • 2 kudos