STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Setting up STM32F765 for dual boot operation.

I'm trying to set up our system for dual boot mode. I'm using AN4826 "STM32F7 Series Flash memory dual bank mode", AN2606 "STM32 microcontroller system memory boot mode", and sample program "STM32F769I_EVAL\Examples\FLASH\FLASH_DualBoot" as guides. ...

murrellr by Associate II
  • 1988 Views
  • 1 replies
  • 0 kudos

Resolved! Hall i2c

hi I'm trying to write some code to read on i2c an as 4058b encoder with the HALL library with stm32, with arduino it works perfectly:Wire.beginTransmission (_slaveAdress);Wire.write (internal_register);Wire.endTransmission ();Wire.requestFrom (_slav...

SDall by Associate II
  • 1265 Views
  • 2 replies
  • 0 kudos

Problem with I2C slave HAL transmit.

I'm tring to transmit as a slave to the master with I2C in a STM32F446RE but i can't get to it.When there is no code running on the MCU i can see the master requesting me to write on the osciloscope. But when I use this code: if(HAL_I2C_Slave_Rece...

Mvega by Associate II
  • 867 Views
  • 0 replies
  • 0 kudos