cancel
Showing results for 
Search instead for 
Did you mean: 

sd card interfacing through sdio+fatfs

Manjesh R
Associate III
Posted on May 09, 2018 at 13:42

hello

     i have been working on file creation on sd card using fat file system,i have got firmware for interfacing using spi, i need firmware using sdio+fats ,if anybody has any idea about this interfacing plz help me out.

                                                                                                                                        thank you

#fatfs #sdio+dma+fatfs #sd-cards
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Posted on May 09, 2018 at 14:20

There are workable software examples for the STM3210E-EVAL

https://community.st.com/0D70X000006SrLUSA0

 

There are schematics for the EVAL board too if you have concerns about the wiring.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Nesrine M_O
Lead II
Posted on May 09, 2018 at 14:40

Hi

manjeshr62

,

I recommend you to have a look to this application under the

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-mcu-packages/stm32cubef7.html

firmware package:

STM32Cube_FW_F7_V1.0\Projects\STM32756G_EVAL\Applications\FatFs\FatFs_uSD

In fact this example provides a description on how to use STM32Cube™ firmware with FatFsmiddleware component as a generic FAT file system module. The objective is to develop an application making the most of the features offered by FatFs to configure a microSD drive.

-Nesrine-

Nesrine M_O
Lead II
Posted on May 09, 2018 at 14:44

example for STM32F1:

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-mcu-packages/patch-cubefw-f1.html

\Projects\STM3210E_EVAL\Applications\FatFs\FatFs_uSD

-Nesrine-

Posted on May 09, 2018 at 14:50

thank you Nesrine M ..I WILL LOOK INTO IT

Posted on May 09, 2018 at 14:52

Manjesh R wrote:

thank you Nesrine M ..I WILL LOOK INTO IT

https://community.st.com/0D50X00009bMM5DSAW