STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can you please let me know if the mapping of LED2 on NUCLEO-H743ZI in code is not done as per the data sheet of the development board?

as Mapping of LED2 is on PE1 in the code for NUCLEO-H743ZI board in ..\en.stm32cubeh7\STM32Cube_FW_H7_V1.5.0\Drivers\BSP\STM32H7xx_Nucleo_144\stm32h7xx_nucleo_144.h file.But the LED2 is mapped to PB7 in the datasheet of the evaluation kit datasheet.B...

VRame by Associate II
  • 1925 Views
  • 5 replies
  • 0 kudos

When using the STM32 Discovery kit IOT node, I am getting the following error " network interface can not be started"

I recently purchased the kit and was using it for first time yesterday. Initially i didnt get the error, I also tried the Wifi-HTTP server example and it worked, but later when i flashed the aws bin file, i started getting this error. Now even going ...

SMann by Associate
  • 634 Views
  • 0 replies
  • 0 kudos

Why does the auido application not work?

HelloI am trying to play the .wav file in this example:C:\Users\user_name\STM32Cube\Repository\ STM32Cube_FW_F4_V1.24.0 \ Projects \ STM32F4-Discovery \ Applications \ Audio \ Audio_playback_and_recordI want to hear the .wav sample is playing, using ...

Cevdet by Associate III
  • 1734 Views
  • 2 replies
  • 0 kudos

STM32 F756, IAP jump to APP issue

I follow the AN4657, use the following piece of code, my IAP can jump to APP when boot up, and APP can jump to IAP. BUT, after jump back to IAP from APP, it will NOT jump to APP successfully.why same code, sometime it works but other time it doesn't ...

HZHU.0 by Associate II
  • 2067 Views
  • 5 replies
  • 0 kudos

Custom USB PD Implementation on STM32G0

Hi everyone,I have been searching for about 3 days straight for a reasonable solution to a USB PD project, and I am still feeling lost. Maybe someone can point me in the right direction.We need to design a USB PD sink circuit which authenticates the ...

TLaux by Associate II
  • 2723 Views
  • 4 replies
  • 1 kudos

Resolved! STM32F411VE - How to use one USB-A connector to read/write flash USB keys and to send/receive data with a PC

Hello everybody,I'm new to USB development then excuse me if my questions are trivial.I have a board with the attached electric scheme (only USB section shown).The application I want to realize must do, with the provided HW, the following:Read/Write ...

0690X000009Z0ixQAC.jpg

USB ZLP send on STM32F429 does not work!

Has *ANYONE* *EVER* gotten USB to work on STM32 without linking in the thousands of lines that Cube framework is?Calling the documentation inadequate is an injustice to that word! The quality of the documentation approaches negative inf! And the cube...

dmitrygr by Associate II
  • 1392 Views
  • 1 replies
  • 0 kudos

Resolved! CDC Device descriptior request failed

I want to realize CDC function to transimit/receive data to/from PC via STM32F105RB. I get the code from Cube. Set clock, enable CDC and modify heap size to 0x1000. But when I power on deivce, "Device descriptior request failed" shown.1.I don't know ...