STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can any STM32's operate USB without HSE?

Hi all,I know the older generations of STM32s cant use USB without the use of an external osc.Has this changed at all with the newer L4, F4, G4, etc micros?Have the HSI's improved enough?Thanks in advance.

mwp by Senior
  • 1178 Views
  • 2 replies
  • 0 kudos

LL drivers UART RXNE interrupt not working.

Hi !I am writing a code that uses the UART1 and I would like to work on RX interrupt to handle incoming strings.To start with it, I wrote a code that simply initialise the UART and send a character once the RX Interrupt is fired:#ifndef HSE_VALUE #de...

simo zz by Senior II
  • 944 Views
  • 0 replies
  • 0 kudos

Resolved! using cdc vcp with adc in dma Mode

Posted on December 17, 2017 at 20:58Hello,i am trying to send data from the adc over the usb otg fs as virtual com port to my pc where i receive the data with a terminal program(HTerm).Using the ADC in 8bit Mode works perfectly. The settings are the...

Resolved! STM32F103RE USB HOST FOR KEY DISK

Greetings Everybody,I am confused whether i cam make STM32F103RE to work as usb host for mass storage ? In CUBE MX it says mass storage class but does it mean i can connect my USB disk to it and transfer data to it ? I know STM32F207ZG has the suppor...

Resolved! DHCP does not work when I change my Mac Address.

 Board: STM32746G-DiscoveryProject: LwIP_HTTP_Server_Netconn_RTOSPosition: ethernetif.c stm32f7xx_hal_conf.h#define MAC_ADDR0  0U#define MAC_ADDR1  2U#define MAC_ADDR2  0U#define MAC_ADDR3  0U#define MAC_ADDR4  0U#define MAC_ADDR5  0UWhen set as abov...

Bootloader behavior

Hi,I need some help to understand the behavior of the bootloader.Currently I use STM32F746 but I will move to STM32F778AI next week.I have several needs from bootloader:Load bootloader if there is no user application.Load user application on start ( ...

davidra7 by Associate II
  • 1246 Views
  • 3 replies
  • 0 kudos

Resolved! Where are the DEMO source project file for the OUT OF BOX demo for the Nucleo-64 STM32F303RE board.

I purchased a Nucleo-64 STM32F303RE for beginning a project. I have downloaded the tools, this includes CUBE_MX and CUBE_IDE. I am able to build a project using these tools as instructed. What I want to know is where is the DEMO project that is loade...

TFlac by Associate III
  • 1448 Views
  • 2 replies
  • 0 kudos

How to restart into bootloader (with DFU).

typedef void resetvec(void);       void cmd_jbl(BaseSequentialStream *chp, int argc, char **argv) // reboot to bootloader   {    unsigned int t;        (void)argc;     (void)argv;    (void)chp;    resetvec *fun;         fun = ((uint32_t *)0x1fffc800)...