STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

why need so many timeout

void sEE_ReadBuffer(uint8_t* pBuffer, uint16_t ReadAddr, uint16_t* NumByteToRead) { //__IO uint32_t timeout = 0xFFFF; __IO uint32_t timeout = 0xFF; /*!< Wait the end of last communication */ for (;timeout > 0; timeout--);   /* Set the point...

I think there is a bug in HAL_TIM_DMABurst_WriteStart (in V1.15 at least), where the timer burst length is used both for the number of registers to write into the timer peripheral and the number of total DMA transfers. Thanks, Aris

There is an identical discussion but for a different mcu:https://community.st.com/s/question/0D50X00009XkdocSAB/timer-dma-burst-mode-arbitrary-waveform

AEfth by Associate II
  • 804 Views
  • 0 replies
  • 0 kudos

Issue with the USB mass storage device class

Hello,We are using STM32L4R5 micro-controller, external NOR flash as a storage media and ST USB device library.We are getting the pop-up as "The last USB device you connected to this computer malfunctioned" on windows 10 system when directly remove t...

Bhushan by Associate II
  • 698 Views
  • 0 replies
  • 1 kudos

How can I use dp83848 for stm32h7?

Hi ,I made ethernet communication with lan8742a phy driver on stm32h743zi but I have to use dp83848 and cubemx doesn't support dp83848 for stm32h7.Is there anyone who can help ?

Bilge by Associate III
  • 1182 Views
  • 1 replies
  • 0 kudos

STM32F777: Strange NETCONN behavior?

Hello!There are two FreeRTOS tasks, each of which creates its own NETCONN object. In one task (the first one begins to execute) there are no oddities when creating a NETCONN object. And in the second task there is: the object returned by netconn_new ...

0690X00000AQuwwQAD.png 0690X00000AQuxLQAT.png
Dimonira by Associate II
  • 686 Views
  • 0 replies
  • 0 kudos

Firmware upgrade problem

How to make DFU jump to a location from where the Factory USB DFU of STM32F070xx resides and it takes control from there? This task is to be achieved using application code instead of the hardware method to pull BOOT0 pin low.We are able to do the Fi...

Resolved! LL drivers PLL initialization

Hi all,I am experiencing some problem with PLL initialization using LL drivers.The code I am using for HSE, PLL and SYS clock is the following:void init_RCC_HSE(void) { //LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOH);   LL_RCC_HSE_Enable(); ...

simo zz by Senior II
  • 1951 Views
  • 4 replies
  • 0 kudos

Resolved! USB Video Class device on L4 HAL library

Hello,I'm working on a DCMI to USB Video Class Device converter for a project of my organization. The image sensor is a ultra low power custom design grayscale level with 640x480 resolution (8 bit per pixel). The DCMI acquisition is working and now I...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.