STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hello. I use CubeMX version 5.2.1, Discovery kit for STM32F7. I try to turn on the Timer1 mode "Combined reset trigger mode" in "one pulse mode" with Trigger source - ITR1(Timer2) One pulse mode does not work. Please help me, thank you.

In the debug mode, timer1 starts, all registers are configured correctly and clocked (CNT, CEN..), but nothing happens on pin TIM_CH1.If I turn off one pulse mode in Timer1 then everything works.Code example:int main(void){ /* MCU Configuration------...

AK.12 by Associate
  • 700 Views
  • 1 replies
  • 0 kudos

Help with STM32F417 MbedTLS support

I am trying to implement a simple MBEDTLS communication firmware with my STM32F417VE.I am using STM32CubeMX as configuration tool and Atollic 9.3.0 as IDE. MBEDTLS, LWIP, FREERTOS and ETHERNET are all set from the STM32Cube.I am trying to perform a s...

NUCLEO-F401RE Serial Port

I have a NUCLEO-F401RE, which has a virtual serial port associated with the built-in ST-LINK/V2-1.This is very convenient and handy, but I'm having issues with it.The first time I tried using this feature, it worked fine. The serial port associated w...

jerry2 by Senior
  • 1737 Views
  • 3 replies
  • 0 kudos

When the server starts up can select - USB - I can see STM32F407 Discovery -VID:115 PID:407). I ok the dialog and Native is Name in Output Tab. I can't upload any designer projects as the designer can not see the board either.

I uploaded the STM32F407 FW to the board, that I downloaded from the website (did not build myself). I have the AWE Designer Version 7.A.0.8 STMicro.I have both USBs plugged in, CM1 at top of board to PC, and CM5 connected to same PC, I can see the S...

mo'br by Associate
  • 665 Views
  • 2 replies
  • 0 kudos