STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Fresh install of CubeMX 5.6 - can't install latest CMSIS, CUBE-LRWAN, MEMSMIC, analog, timcooker libraries - all report .pdsc failure?

Trying to do a build of STM32L073, with latest CMSIS, LRWAN, MEMSMIC, and other libraries, but all seem to fail install into CubeMX on Win10. All install attempts report some .pdsc database failure. This is a new / clean install, and trying to add pa...

TZiel.1 by Associate II
  • 1061 Views
  • 0 replies
  • 0 kudos

STM32L151CCT7 USB bootloader enter/leave DFU lockup

We used the STM32CubeMX program to generate a USB Custom HID. The program works and we can leave the application and enter the bootloader. The BOOT0 pin is high and the BOOT1 pin is low so it always runs the bootloader from reset. We then tell it to ...

MSt. .1 by Associate
  • 733 Views
  • 0 replies
  • 0 kudos

How to have access to the output data of the 2 digital microphones of the STM32L475VGT6 device (Discovery kit) ?

Hi,I'm working on a project where I need to make "sound recognition". In my case, I have to detect the nature of an object (paper, metal, glass etc.) based on its sound. To do that I envisage to use deep learning and thus to use the STM32CubeAI p...

Lionel_D by Associate II
  • 1647 Views
  • 1 replies
  • 0 kudos

I want to add a USB CDC driver to my application on a STM32F446 (self powered device). However, I had to use the dedicated VBUS pin for another function.

According to https://community.st.com/s/article/FAQ-Management-of-VBUS-sensing-for-USB-device-design the software handling of VBUS presence event needs to be implemented by the customer.How can I implement VBUS sensing on another pin SW wise? VBUS i...

Marcus1 by Associate II
  • 1802 Views
  • 4 replies
  • 0 kudos

Resolved! STM32 Ethernet

I use ethernet switch instead of PHY with stm32f4. While RMII pins are connected to STM32, I manage MDIO pins with SPI.There is basic things whic is I can not understand.What is the difference between the autonegation,speed settings in STM32 ethernet...

DCtech by Associate II
  • 1224 Views
  • 1 replies
  • 0 kudos

STM32F407 OTG usb storage driver pin alternative

Hi,My OTG (CN5) socket was damaged so i checked pinout of the board to find alternative pins to connect new OTG socket on a separate pcb and i found pins (PA9 , PA10, PA11 and PA12) for FS mode but unfortunately PA11 and PA12 are not mounted on the S...

Aabda.1 by Associate
  • 726 Views
  • 0 replies
  • 0 kudos