STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using USB Vendor ID from ST

Hello together,We planned to use for our product the following MCU: STM32L4A6RG.So is it possible to use the USB Vendor ID from ST if I implement in the Firmware a Virtual COM Port over USB interface? I know that I can use the USB VID for evaluation ...

DMark by Associate II
  • 1768 Views
  • 4 replies
  • 0 kudos

Azure FOTA on STM32L475

Dear friends,I am facing one issue with FOTA on Azure platform.We are trying with evaluation kit (B-L475-IOT01A2)The errors seen are Download FOTA from: HostName=[stm32blob.blob.core.windows.net] Type=[Secure] port=[443] File=[/firmware-nucleo/Azur...

Raju1 by Associate
  • 385 Views
  • 0 replies
  • 0 kudos

U(S)ART ORE hits again, STM32H7

Have read about the ORE interrupt problem on STM32F7.On STM32H7 it looks like the overflow condition prevents setting RNE flag, even in polling mode, without any involvement of interrupts.With the current H7 HAL driver v 1.5.0, it is very simple: cal...

Pavel A. by Super User
  • 575 Views
  • 0 replies
  • 0 kudos

STM32F7 eMMC FATFS writes data speed only 585KB/S

Hi ST communities,My hardware is MCU STM32F756, eMMC mtfc2gmdea-0m 4bit 24MHZ CLK.FATFS: R0.12C.STM32F7_Cube_FW_Ver:STM32Cube_FW_F7_V1.15.0.Why does eMMC now write data at only 585KB/S. FATFS_WR_SIZE 8192, every time to writes 1024Bytes.uint8_t wtext...

ddavi.8 by Associate II
  • 1008 Views
  • 2 replies
  • 0 kudos

HAL CubeMX I2C slave NACK problem (STM32F446)

Technical environment :-       Master : CM3 (Raspberry)-       Slave : STM32F446-       CubeMX : V4.23 (even tested with V4.26.1)-       Normal transaction is : MASTER do a 4 bytes WRITE, then a 1 byte WRITE and at last, a 4 bytes READ.The slave ACKe...

0690X000006By7MQAS.png
YBOUR by Associate II
  • 2756 Views
  • 6 replies
  • 0 kudos