STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H747I-DISCO with LWIP not working

Hi, I am working with STM32H747I-DISCO but the lwip not working. I have apply the recommendations here https://community.st.com/s/article/FAQ-Ethernet-not-working-on-STM32H7x3 but the LAN8742.c have infinity loop in line 170. while(regvalue & LAN8742...

Resolved! Stm32f405 unable to enter DFU

I have designed my custom stm32f405 board based on Pyboard 1.1 and Adafruit Feather stm32F4 Express and was unable to enter USB DFU with it.I uploaded the code using ST-Link and can confirm that USB OTG FS works, without DFU the device is visible as ...

0690X00000ByaESQAZ.png
DLegu.1 by Associate II
  • 3420 Views
  • 5 replies
  • 0 kudos

B-L072 Discovery Board - DFU Mode

Hey guys, I am seeking to activate the DFU mode in the B-L072 Discovery Module using the Murata CMWX1ZZABZ-091 module.I have kept BOOT0 pin to HIGH and connected a USB cable to the CN11 USB connector. But STM32prog does not detect the DFU bootloader....

stm32f105 Device Only issues

HII am struggling to set up USB Device only on stm32f105I do set up followingRCC - Crystal resonatorSYS - Debug Serial wireUSB_OTG - Device onlyUSB Device - CDCClock I set up 8MHz and run resolveBuild project and load firmwareAnd after connecting to ...

AMaka.1 by Associate II
  • 414 Views
  • 0 replies
  • 0 kudos

USB host HID stops t APPLICATION_START

HiI have issue with setting up USB Host HID on Stm32f105. It is simple circuit only 8Mhz crystal and 2 22pF caps. And USB port.​I did set up RCC, usb to host only, and HID interface​.After generating code I can see that state machine is changing on i...

AMaka.1 by Associate II
  • 649 Views
  • 1 replies
  • 0 kudos