STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is it possible to use the STLINK (V3) that's integrated into some of the Nucleo boards to program external devices?

I have an NUCLEO-G474RE that I used for prototyping, and now I also have a custom board with a G474 on it that includes a MIPI10 debug connector. I can program and debug with the standard STLINK-V3SET just fine. However, I would like to know if it is...

JQuan by Associate II
  • 1257 Views
  • 1 replies
  • 0 kudos

Resolved! Where to buy a STLinkV3 MODS board ?

I designed a pcb adapter for this board in order to use it with my V2 based project, I’ll received soon this pcb from JLCPCB but I find no way to buy a board :ST website distributor stock informations are wrong, Digikey as 0 in stockFarnell has’nt go...

AIM65 by Associate III
  • 4849 Views
  • 13 replies
  • 0 kudos

Resolved! How to make a Nucleo Board visible via USB?

I want to flash my Nucleo Board from STM32CubeIDE. When I click debug in the IDE it fails with:ST-Link enumeration failed   Error in initializing ST-LINK device. Reason: ST-LINK DLL error.st-info --probe saysFound 0 stlink programmersWhen I enumerate...

cqexbesd by Associate II
  • 4465 Views
  • 3 replies
  • 0 kudos