Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

S2-LP Gm Crit Value

 We have a problem to drive a crystal some of the PCB on after the mass production as we tought have problem to value of XO_RCO_CONF0  registers GM_CONF values.Is there any body help that value?How can we solve that problem?Is this value critical? No...

Resolved! STKNX Buck converter don't get 12V output

I am trying to get 12V at the output of STKNX buck converter, but I am not getting it and the STKNX dead.The RFB1 that I am using is 33K Ohm and the RFB2 is 3k Ohm, with these resistors the Vout would be 1 + 33k/3k = 12V. The maximum value of this vo...

IO-Link slave protocol stack for object-oriented programming portable to any MCU platform,portable IO-Link communication master station

Background:        I have implemented an IO-Link communication slave device using IO-Link PHY chips such as L6362. After multiple rounds of object-oriented code organization。The MCU resource driver, IO Link slave protocol stack, and PHY chip were abs...

STEVAL-IDP004V2

Hello, I am experiencing issues with my STEVAL-IDP004V2 evaluation board. When I connect the device to my  computer, it is not recognized properly. Attempted to update the USB drivers through device manager, used different USB ports and cables. Where...

bobrzyn by Associate
  • 920 Views
  • 0 replies
  • 0 kudos