User Activity

Hi,I am trying to install a Lorawan network server on a local computer following the instructions provided here: How to create a LoRaWAN server on local PC (1/2) - STMicroelectronics CommunityI am installing it on a Window 10 machine, and had an erro...
Hi,There is an introduction on the EVKITST87M01 development kit in the flyer found here: fl2311st87m01.pdf, however, I could not find anywhere online to purchase it. Just wondering if it is available yet?Thanks,Olive
Hi,I have a device that is integrated with BlueNRG-LP chip for BLE communication. The client side is an app implemented in python on windows 10. After connection is established, data starts to be transmitted from the BlueNRG-LP to the computer, howev...
Hi,I have two GPIO pins on BlueNRG-LP connected to the reset and CS on a potentiostat device. The reset and CS need to be kept high during BlueNRG-LP deep sleep mode. Just wondering how to keep these two pins active while the BlueNRG-LP is put into d...
Hi,I am trying to transfer 2k bytes data every a while (20s for example) from BlueNRG-LP to my computer with one connection event. the 2KB data is divided into 5 chunks (data packets), which means 5 data packets contain a complete data set.  After I ...
Kudos given to