yyys
Associate II
since
2024-01-26
2024-03-19
User statistics
4
Posts
1
Solutions
0
Kudos given
0
Kudos received
View all badges
STMicroelectronics Community
About yyys
Options
Report User
User Activity
Posts
Replies
BlueNRG-LPS HID change made chip restart
2024-02-21
I change the HIDdescMap to uint8_t reportDesc[] = { 0x05, 0x01, // Usage Page (Generic Desktop) 0x09, 0x06, // Usage (Keyboard) 0xA1, 0x01, // Collection (Application) 0x05, 0x07...
a problem about BLE_HID_Peripheral
2024-01-26
I am using the blue-nrg-lps,but when i test the hid example project , it cannot work in win11,but it is ok in phone and pad,so anyone can tell me why? A new player of ble-nrg-lps...
Re: BlueNRG-LPS HID change made chip restart
2024-02-21
question was be solvedjust because i donot remind the max len of the report pack#define REPORT_MAP_MAX_LEN 80 => #define REPORT_MAP_MAX_LEN 480
Re: BLUENRG-LP BLE HID KEYBOARD with WINDOWS 10 PC
2024-01-26
I tested your way,it cannot work. can you send a proj to my email?