Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Dev.Kit STEVAL-BFA001V2B - IOLink

Hi,I am testing the STEVAL-BFA001V2B development kit to evaluate the use of the IOLink protocol. Using the native project provided in the software package for the STide development environment, the device connects to the master and works correctly. T...

padovmar by Associate
  • 822 Views
  • 0 replies
  • 0 kudos

Resolved! STW81200 does not answer on MISO line

Hi, Im interfacing STW81200 with SPI without no success. I do have the following questions:What the SPI mode? Its not clear on the datasheet. It seems that CPOL = 1, and CPHA = 1.In either way, I have tested the communication with several modes and n...

Question about using DCMI in extra ADC(AD7768)

我尝试使用 STM32L4R9 与 AD7768 通信,使用 8 个通道。我想知道的是:是否可以使用 DCMI 建立 AD7768 与微控制器之间的通信(微控制器支持,但我不确定 AD7768 是否支持 DCMI。)如果 AD7768 也支持,我想知道 PCB 应该如何正确布线。Translation to English I am trying to communicate with the AD7768 using the STM32L4R9, using 8 channels. What ...

maya123 by Associate II
  • 974 Views
  • 0 replies
  • 0 kudos

STPM34 (EVALSTPM34) - After HPF is disabled, why did we failed to read the V-I channel's DC offset of V / C channels?

Hi,     We try to use STPM34 to measure DC V and I inputs besides measuring AC. The HPFs of V1,V2/C1,C2 on the EVALSTPM34 board were disabled by sending {0x00, 0x01, 0x18, 0x04, 0x88} and {0x02, 0x03, 0x18, 0x24, 0x92} to STPM34 through SPI.         ...

spirit1 auto retransmission and auto ack

Posted on May 14, 2014 at 19:25Hi, My Interesting is the next, how can I use Spirit1 Auto retransmission and auto ack abilities in half duplex communication. My coordinator is supplied with main power, but nodes are powered by alkaline batteries. Th...

szabo by Associate
  • 2691 Views
  • 5 replies
  • 1 kudos