Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! EVAL-SCS001V1

I am hoping to understand whether or not this STUSB4500 PD controller on this evaluation board will default to a 5V sink level if it attaches to a standard USB-A port that does not communicate over the CC lines. I have tried this with a USB-C PD sour...

marke by Associate
  • 845 Views
  • 1 replies
  • 0 kudos

Spirit1 undocumented registers

In the Spirit1 driver code, two registers at address 0x99 and 0x9A are being written.These don't appear to be documented anywhere. Does anyone know what they do?This is the code fragment:/* Set the IQC correction optimal value */anaRadioRegArray[0]=0...

chazzab by Associate
  • 524 Views
  • 0 replies
  • 0 kudos

STEVAL-MKI2231K

HelloI need help with STEVAL-MKI109V3 and STEVAL-MKI223V1KThe error message is:The sensor has not been recognizedThe WHOAM_I register value does not match the device selected.

JoseD by Associate
  • 887 Views
  • 1 replies
  • 0 kudos

Resolved! Documentation error: TCPP01-M12 datasheet

Hi,I am currently working with the documentation of TCPP01-M12. I have find some small mistake in the table of recommended capacitor C3. The part codes are switched. Also it seems that the GRM188... 0603 package capacitor is obsolete nowadays. Could ...

Datasheet- TCP01-M12.PNG
Marosh by Associate III
  • 2739 Views
  • 2 replies
  • 3 kudos