Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STPM34 weird values reading his registers

Hi, I'm debugging a board with two STMP34 used to read voltage and current from L1 - L2 and L3 of a threephase system.  The current signals comes from three different TA devices. The issue is: sometimes, reading a block of registers using the Metro_H...

SteRogge_2-1726839139781.png SteRogge_1-1726838870158.png SteRogge_4-1726839712971.png SteRogge_3-1726839290450.png
SteRogge by Associate
  • 581 Views
  • 0 replies
  • 0 kudos

Resolved! BlueNRG-LP certification BQB

Hello,I hope you are well.I have a question about the certification of the “Programmable Bluetooth® Low Energy wireless SoC” from the “BlueNRG-LP” family: are they BQB certified?Thanks in advance

ljm by Associate III
  • 1511 Views
  • 1 replies
  • 1 kudos

S2LP very low RX sensitivity

I've bought a S2LP dev board STEVAL-FKI433V2 as I'm evaluating the S2LP for a product revamp.Because it will be used with a legacy system I want the receive side to completely bypass the packet decoding and output to GPIO - which seems to work to a p...

Nik100 by Associate
  • 970 Views
  • 1 replies
  • 0 kudos