I am MURAL SELVAM from India. I am Currently working on Automotive project I need reference Design for Below given part number..SPC560D30L1B4E0XIf You have any reference design kindly provide me.
Hi, I am MURALI SELVAM from DNCL Technologies, I need reference schematic for STM32G0B1VET6 MCU, If anyone have reference schematic. Kindly provide me. Thank you.
Hi, (STM32G0C1RET6 for this part number ARM® Cortex®-M0+ STM32G0 Microcontroller IC 32-Bit Single-Core 64MHz 512KB (512K x FLASH 64-LQFP (10x10))two type of pin descriptions have mentioned in the datasheet, I confused which one I have to ...
Hi, I am Murali Selvam from India, I have a doubt, Can we interface the external Micro-SD card through below given MCU, You have any reference schematic kindly give me. Thank you.
STM32G0B1KBU6,STM32G0B1KET6
Hi, I am MURALI SELVAM from India, We are plan to build the circuit for Battery Monitoring circuit for which I select L9963E so someone give me suggestion for ensure L9963E part number is suitable for my project, My battery spec is "6S 25200 mA/h so ...
Hi, Karl Yamashita.. I understand you reply and I am new in CAN protocol so I have one doubt, Shall I use this CAN protocol for hear beat signal generation, For example One MCU can work in up to 250Mhz for timer, How much frequency I nee...
in my project I will go to use three MCU, master one is fail, 2nd slave will take control, 3rd one is should not take control, 1st and 2nd failure that time only 3rd one will take control. This logic going to implement. is that possible for heart bea...
I plan to implement heart beat signal through SPI protocol so generally I want know about how to implement and perform heart beat signal so that asked you.
Can I use CAN protocol for generating heart beat signal (you have any paper about heart beat signal kindly share me)? it will work perfectly? if The three MCUs are connected with CAN protocol, one MCU will get failure another MCU will take control is...