cancel
Showing results for 
Search instead for 
Did you mean: 

Recommendations for how to program BlueNRG-M2SP in production

KKram.1
Associate

These answers say that the BlueNRG-M2SP module comes blank and must be programmed with a firmware binary.

https://community.st.com/t5/interface-and-connectivity-ics/preloaded-firmware-of-bluenrg-m2sp/m-p/134698#M1534

https://community.st.com/t5/interface-and-connectivity-ics/what-mode-is-the-bluenrg-m2sp-module-in-when-its-comes-from-the/td-p/657978

How do you recommend the BlueNRG-M2SP module be programmed in a production environment?  For example, are there tools available for pre-programming the module before it's soldered to the custom board?  Or does the module need to be programmed in circuit through the module's SWD connection with tools such as ST-Link V2 and the programmer application?  Programming in-circuit with ST-Link might be OK for low volume production but is there a better solution for high-volume products?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Uwe Bonnes
Chief

I think, ST can offer devices programmed to you spec. And there are 3-rd parties that can program for you. Otherwise to the pogrammin during boar test.