Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG-2 pins for UART comms

I have a custom-built board with a BlueNRG-2 chip on it. The BlueNRG-2 chip is flashed with the UART version of the binary provided in the STM32CubeExpansion_BLE2_V1.0.0 package.Can anyone provide me the pins that the BlueNRG-2 uses for its UART comm...

SBukh.1 by Associate II
  • 581 Views
  • 0 replies
  • 0 kudos

IDB008v2: No ST-LINK detected

Hello everyone,I just got an IDB008v2 evaluation board and I'm having some issues setting it up and programming it.I can flash some demo programs from the BlueNRG-2 Navigator, which works (Tera Term receives the print messages and BLE scanner app see...

RCler.11 by Associate
  • 2090 Views
  • 3 replies
  • 0 kudos

SPBTLE-RF0 sending stale data

In our application spbtle-rf0 is used to communicate with android app.​ when data is sent, some times it is observed that part of the previous data is transmitted. The data is split into 20 bytes packet. When it is configured as indicate some times t...

AKall.1 by Associate
  • 702 Views
  • 0 replies
  • 0 kudos

Spbtle-rf0

In our application spbtle-rf0 is used to communicate with android app.​ when data is sent, some times it is observed that part of the previous data is transmitted. The data is split into 20 bytes packet. When it is configured as indicate some times...

AKall.1 by Associate
  • 570 Views
  • 0 replies
  • 0 kudos

Python support on BlueNRG1

Hi there,I programmed BlueNRG1 with bluetooth stack in C language. I want to know, about the support of python for BlueNRG1. As now a days, their are many controllers supporting micropython. Is their some sdk available for ​this SoC.Thanks & RegardsS...

SPras.1 by Associate
  • 687 Views
  • 0 replies
  • 0 kudos

I2C communication error with STUSB4500

Hi Community, I have a STREF-SCS001V1 board and I try to create communication with STUSB4500 IC via I2C, but there is no response. I tried to sweep addresses from 0x00 to 0xFF but there is not hit for any address. Also I tried 0x50 and 0x51 alone but...

Andras by Associate
  • 829 Views
  • 0 replies
  • 0 kudos