cancel
Showing results for 
Search instead for 
Did you mean: 

BLE communication is not working on Customize board.

Skada.3
Associate III

Hi

I have made customize board with the reference of STM32l476RG Nucleo Board and X Nucleo IDB05A1.

Board is working fine with the example project of 'STM32CubeExpansion_BLE1_V4.4.0', but having issue with 'STM32CubeFunctionPack_BVLINK1_V1.0.0'. When I am using example project of 'BVLPer', the board fails to advertise.

In both examples pin configurations are same for BLE module, but still getting the different output from the same module.

Looking for solution.

Thank you in advance.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0