Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How can I connect dualshock3 to f7 with cube Ide?

I am trying to connect dualshock3 to stm32f746zg these months. I heard f7 has pins which fit to Arduino so I bought usb host shield 2.0 (for Arduino) and a bluetooth donglel. I know some people use Arduino Ide and run with this shield.but how can I r...

T22 by Associate II
  • 1115 Views
  • 2 replies
  • 0 kudos

[BlueNRG-1/2] Normal guide on programming?

After almost half of a year working with your BlueNRG products I'm still wondering how I am supposed to program it normally.I usually use your examples to make a solution, but it is fairly not enough.Peripheral examples are obsolete and mostly useles...

DB.2 by Associate
  • 663 Views
  • 0 replies
  • 0 kudos

BLE SW stack and profiles

I looked at BlueNRG 1 and consider what SW there is from ST. Can you point me to a description of what is delivered and the conditions?Do I need to involve 3rd parts here or do ST deliver all and support the BT stack and profiles?

Epoul.1 by Associate II
  • 700 Views
  • 0 replies
  • 0 kudos

BlueNRG-1 Advertising stops

Hi, i`m having an issue with BlueNRG-1. It is configured to advertise every 10 seconds. However, advertising stops after hours, and I can´t connect to the device again. I can see no radio activity on spectrum analyzer when this happens. Any idea abou...

MHere.1 by Associate
  • 660 Views
  • 0 replies
  • 0 kudos

How check Ethernet? I'm receiving frames on RXD0, RXD1 and assertion of CRS_DV (RMII interface) but any connection can be performed.

Hello, I have designed a PCB with a STM32F746VET6 microcontroller and LAN8742A physical interface and magnetics. I'm not an expert in Ethernet and I'm not achieving to make it works. I want to validate this design and I'm trying to do a ping to the d...

Luis Ber by Associate II
  • 1286 Views
  • 0 replies
  • 0 kudos

BlueNRG-2 - how to switch on the LS RO oscillator with working LS XO oscillator without external reset (RESETn pin) or power cycling after firmware updating over "OTA"? The chip is BlueNRG-232 (it reports a "chip version" 1.0.0).

We use BlueNRG-2 in custom sensor. The original firmware uses LS XO (32 kHz crystal). But we need to have ability to choose the LS "RO" or "XO" after firmware updating over "OTA" (FOTA). It seems that if LS XO has been turned on once then the LS RO i...

SPopo by Associate
  • 619 Views
  • 0 replies
  • 0 kudos

BLE Mesh on BlueNRG-1 w/Proxies?

I have an existing phone app (using the traditional GATT system), and I would like mesh-enable my products so that if the products can see each other, then the phone can connect to and control any node (so, not so much an automation system but a rela...

TJohn.14 by Associate II
  • 705 Views
  • 0 replies
  • 0 kudos