Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STPM34 Init Issue

Hi. I am using two STPM34 on my board, they are separated, UART, SCS, SYN, all of them. I got init issue happens at start-up. I can't detect it. I've applied this Getting started with the STPM3x document procedures and got driver code that provided b...

yucelc_1-1743767310012.png
yucelc by Associate
  • 661 Views
  • 0 replies
  • 0 kudos

BLUENRG_LP GATT Service Crash

platform:BLUENRG345_MCSDK :BLUENRG_LP_1.2.0Our device serves as a broadcaster (directional broadcast), with GATT acting as a server, providing one service and two characteristics(read_req and WriteReq). The target device will periodically connect to ...

CYHHF by Associate
  • 795 Views
  • 0 replies
  • 0 kudos

X-NUCLEO-S2915A1

Hello everyoneDo you know where can I find a ready to use example for X-NUCLEO-S2915A1 . It seems that everything is for other boards.I also tested P2P example from cube for L1 ("S2915A2_P2P") and it doesn't work . Two boards I press the button and n...

JesusAVC by Associate II
  • 540 Views
  • 0 replies
  • 0 kudos

blunrg2 and indication

Hallo, I have in my middlewares BluNRG2 packet.I have this function aci_gatt_add_char that adds a characteristic that has ((uint8_t)CHAR_PROP_NOTIFY)|((uint8_t)CHAR_PROP_READ | CHAR_PROP_INDICATE) as Char_Properties.When this characteristic changes, ...

IVent.1 by Senior
  • 530 Views
  • 0 replies
  • 0 kudos

BLE Mesh

hello, as part of a project for a course I'd like to recover the sound intensity in random places. For this, I have 3 steval mksbox1V1 and I use the microphone mp23abs1 to recover the sound intensity in db of an environment. I'd like to place the car...

Issues with STPM34-EVAL Board.

Hello Team,We have a STPM34-EVAL board and we are trying to interface 220V AC with it, Earlier the software worked well and were able to see all correct values, Now voltage seems to be messed up. Current detection is fine.Will you be able to provide ...

STiD135

Hello Community.I have been trying for months now to get info on the STiD135. I realize it's discontinued but WHY????Did SAT>IP fail? The SAT>IP protocol, introduced in 2012, aimed to revolutionize satellite distribution by converting DVB-S/S2 signal...

STuW81300 power control

Hello, It looks like the synthesizer STuW81300 has RF power degradation across frequency (power is +4dBm at 4GHz and -4dBm at 7.5 GHz). We can't reach declared in data sheet +8dBm at RF1_OUT. How we can control RF power for STu81300 e.g. similarly as...

AStre by Associate III
  • 1208 Views
  • 1 replies
  • 0 kudos